SLIA097 March 2022 DRV5011 , DRV5011 , DRV5012 , DRV5012 , DRV5013 , DRV5013 , DRV5015 , DRV5015 , DRV5021 , DRV5021 , DRV5023 , DRV5023 , DRV5032 , DRV5032 , DRV5033 , DRV5033 , TMAG5110 , TMAG5110 , TMAG5111 , TMAG5111 , TMAG5123 , TMAG5123 , TMAG5231 , TMAG5231 , TMAG5328 , TMAG5328
With the impeller and flow meter body assembled, the two components can now be joined together. Install the impeller onto the steel shaft located in the flow meter body. Proper assembly should allow the impeller to now rotate freely. Additionally, the bottom bearing should hold the impeller slightly above the bottom of the flow meter body to reduce friction. If the bearings do not easily assemble onto the shaft, it may be necessary to reduce the outer diameter of the shaft. Reduce the outer diameter of the shaft by cooling the steel shaft in a freezer for enough time to allow the bearing to slide onto the shaft. Figure 3-4 displays the properly assembled components.