SLIA097 March 2022 DRV5011 , DRV5011 , DRV5012 , DRV5012 , DRV5013 , DRV5013 , DRV5015 , DRV5015 , DRV5021 , DRV5021 , DRV5023 , DRV5023 , DRV5032 , DRV5032 , DRV5033 , DRV5033 , TMAG5110 , TMAG5110 , TMAG5111 , TMAG5111 , TMAG5123 , TMAG5123 , TMAG5231 , TMAG5231 , TMAG5328 , TMAG5328
Omnipolar switches act as two opposite polarity unipolar switches connected together. Therefore, the switch still operates using BOP and BRP; however, the polarity of the B-field no longer influences the output of the sensor. This implementation requires the magnets be positioned far enough apart to allow the B-field to fall below the BRP threshold between magnets. Use of the omnipolar switch enables the magnets to be positioned in any orientation (North facing or South facing) with no polarity influence to the sensor operation. Magnets can be positioned in either orientation, simplifying overall mechanical assembly of the flow meter. Omnipolar switch operation is displayed in Figure 2-4.