SLLA521B January 2022 – June 2022 TCAN1145-Q1 , TCAN1146-Q1
The TCAN114x-Q1 can be configured to either ignore CAN-FD frames (no change to the error counter) by setting SW_FD_PASSIVE=1 to enable FD Passive mode, or treat them as error frames (increment the error counter) by setting SW_FD_PASSIVE=0. Most applications will prefer to ignore CAN-FD frames and use the FD Passive feature. As the CAN-FD frame format is different than a Classical CAN frame format following the FDF bit, the internal frame decoder will ignore the remaining part of the CAN-FD frame by waiting for the next Bus Idle, indicated by a run of six recessive (1) bits.