SLLA535 December 2022 TLIN1431-Q1
The TLIN1431x-Q1 component is targeted at general-purpose functional safety applications utilizing SPI control. This is called Safety Element out of Context (SEooC) development according to ISO 26262-10. In this case, the development is done based on assumptions on the conditions of the semiconductor component usage, and then the assumptions are verified at the system level. This method is also used to meet the related requirements of IEC 61508 at the semiconductor level. This section describes some of the target applications for this component, the component safety concept, and then describes the assumptions about the systems (also known as Assumptions of Use or AoU) that were made in performing the safety analysis.
Example target applications include, but are not limited to, the following:
Figure 4-3 shows a generic block diagram for a general purpose system. This diagram is only an example and may not represent a complete system. Figure 4-4 provides potential failure points that have diagnostic or test ability mechanisms.
Potential Failure Point from Figure 4-4 | Potential Failure Point Description | Section |
---|---|---|
1 | LIN communication | Section 6.3.1 |
2 | Supply voltage rail monitoring | Section 6.3.2 |
3 | SPI/Processor communication | Section 6.3.3 |
4 | Floating pins | Section 6.3.4 |