SLLA535 December 2022 TLIN1431-Q1
The TLIN1431x-Q1 LIN transceiver is a Local Interconnect Network (LIN) physical layer transceiver, compliant to LIN 2.0, LIN 2.1, LIN 2.2, LIN 2.2A and ISO/DIS 17987–4 with integrated wake-up and protection features. The LIN bus is a single-wire, bi-directional bus that typically is used in low speed in-vehicle networks with data rates that range up to 20 kbps. The device LIN receiver works up to 100 kbps supporting in-line programming in normal mode. When the device is placed into fast mode both the transmitter and receiver supports up to 200 kbps. The device converts the LIN protocol data stream on the TXD input into a LIN bus signal using a current-limited wave-shaping driver which reduces electromagnetic emissions (EME). The receiver converts the data stream to logic level signals that are sent to the microprocessor through the RXD pin. The LIN bus has two states: dominant state (voltage near ground) and recessive state (voltage near battery). In the recessive state, the LIN bus is pulled high by the internal pull-up resistor (45 kΩ) and a series diode.
Ultra-low current consumption is possible using the sleep mode. The TLIN1431x-Q1 provides three methods to wake up from sleep mode: EN pin, WAKE pin and LIN bus in pin control mode and two in SPI control mode, WAKE pin and LIN bus. The device integrates a low dropout voltage regulator with a wide input from VSUP providing 5 V ±2.5% or 3.3 V ±2.5% with up to 125 mA of current depending upon system implementation.
The TLIN1431x-Q1 integrates a window based watchdog supervisor which has a programmable delay and window ratio determined by pin strapping or SPI communication. The device watchdog is controlled by pin configuration or SPI depending upon the state of pin 7 at power up. At power up, if pin 7 is externally pulled to ground, the device is configured for pin control of the device. If pin 7 is left floating or pulled up to VCC the pin becomes the nCS pin from the processors for SPI communication. If the pin is left floating at power up, the internal pull up configures the device for 3.3 V SPI control. If the processor uses 5 V IO a 500 kΩ pull up resistor to VCC is used for the 5 V version of the device. This allows the 5 V version of the device to work with both 3.3 V SPI or 5 V SPI. SPI communication is used for device configuration. In pin configuration nRST is asserted high when VCC increases above UVCC and stays high as long as VCC is above this threshold.
When the watchdog is controlled by the device pins, the state of the WDT pin determines the window time. WDI is used as the watchdog input trigger which is expected in the open window. If a watchdog error event takes place, the nWDR pin goes low to reset the processors. When using SPI, writing FFh to register 15h, WD_INPUT_TRIG, during the open window restarts the watchdog timer. The supervised processor must trigger the WDI pin or WD_INPUT_TRIG register within the defined window. When using SPI, the nRST pin can become the watchdog event output trigger for the processor if programmed this way but the nRST function are lost. The watchdog timer has a long initial window when entering standby, normal and fast modes that a watchdog input trigger is expected.