SLLA541 December 2020 TCAN1144-Q1 , TCAN1146-Q1
A FMEDA is a common functional safety analysis technique used to determine the effectiveness of a functional safety architecture. For failure modes of the design blocks identified, a probability of occurrence is quantified. For diagnostics implemented, the effectiveness of the diagnostic is quantified. The quantification of these values enables the calculation of safety metrics per targeted functional safety standards such as the IEC 61508 safe failure fraction or the ISO 26262 single point fault metric, which estimates the effectiveness of the implemented safety architecture.
TI has created a FMEDA for this device that allows the user to tailor the metrics to their specific use case based on which features or design blocks are being used as part of the safety function. This tool additionally allows the user to modify the environmental factors, device power consumption, and other factors that affect the raw (base) FIT rates. Finally, this tool allows the user to customize the diagnostics that are applied that can detect faults within the device itself. All of the green cells in the spreadsheet can be modified by the user. All other cells have been populated by TI based on the specifics of the device or are calculated based on the user selections. This Excel workbook is locked to protect the user from incorrectly modifying the calculations. The sections below go into detail on how to use these tailoring options. Any tab not mentioned below is informational.
See Section 2.3.1 for the default values of these fields in this device's FMEDA.