SLLA541 December 2020 TCAN1144-Q1 , TCAN1146-Q1
The user is expected to tailor this sheet to their specific use-case.
The 'Function and Diag tailoring' tab takes the raw (base) permanent and transient rates and distributes them among each of the design blocks (sometimes referred to hardware elements or IPs) of the device. Each row represents the lowest part of this analysis and each row gets a percentage of the FIT based on its transistor count or memory size. The user should refer to the Safety Manual in combination with this FMEDA to determine which design blocks are used in their application for a safety-related function. The design blocks that are not used can be marked as "No" for "Safety related HW element to be considered in the analysis?". This will remove these rows from the FIT calculation, which affects the safety related FIT and all derived metrics. Additionally, a set of Safety Mechanisms can be applied to each row to provide diagnostic coverage for faults associated with its function (please note that each selection here represents multiple safety mechanisms applied. For each row, the diagnostics that are applied to provide coverage for permanent faults, transient faults, and latent faults are split into separate columns so that the diagnostics can be applied to each. The list of Safety Mechanisms can be found in the 'Diagnostic Coverage' tab. TI may pre-populate the function and diagnostic tailoring selections in based on one or more expected use cases for the device. Altering the selection of Safety Mechanisms will impact the Probabilistic Metrics for random Hardware Failures (PMHF) and Single Point Fault Metric (SPFM) in the 'Totals - ISO26262' tab or the Probability of Hardware Failures (PFH).
The definition for each row in this FMEDA can be found in the Description of Hardware Component Parts chapter of the device safety manual in addition to the diagnostic options available and the full list of diagnostics available. For additional guidance on how to determine which parts are related to the system safety function, refer to 'An In-Context Look at this Safety Element out of Context' chapter of the Device Safety Manual as well.