SLLA549 July 2021 TCAN4550 , TCAN4550-Q1 , TCAN4551-Q1
All trademarks are the property of their respective owners.
The TCAN455x family of devices uses a Pierce oscillator based design that operates in the inductive region between a crystal’s parallel and series resonant frequencies for a wide range of quartz crystals up to 40 MHz with a maximum ESR of 60 ohms and with load capacitance (CL1=CL2) requirements ranging between 8 pF and 24 pF. It is also capable of operating with a single-ended clock source instead of a quartz crystal supplied to the OSC1 pin, automatically detecting when a single-ended clock is used, and disabling the quartz crystal amplifier and biasing circuit.
This design creates flexibility for how the device is used in the end application, but results in a few additional design requirements that need to be understood to ensure stable operation. This document discusses these requirements and serves as a guide on optimizing the oscillator clock circuit components.
A crystal-based oscillator is formed by placing a crystal in the feedback loop of an oscillator circuit that provides sufficient gain and phase shift around the loop to start and sustain stable oscillations. A detailed explanation of crystal oscillator operation will not be covered here. However, to support the reader’s interpretation of the guidance and recommendations contained in this application note, some essential aspects of the crystal oscillator circuit model are presented and explained here. A simple model of a crystal is shown in Figure 2-1. The model has R-L-C series components, called motional resistance (Rm), motional capacitance (Cm), and motional inductance (Lm). The capacitor in parallel, C0, is called the shunt capacitance, and models the package capacitance. Figure 2-2 illustrates a simple oscillator model, consisting of an inverting amplifier and crystal, and its equivalent circuit model.
The circuit model in Figure 2-2 is useful for understanding the necessary conditions for oscillation. These are:
Where:
XXTAL = the imaginary part of the impedance represented by the crystal.
RXTAL = the real part of the impedance represented by the crystal.
XOSC = the imaginary part of the impedance represented by the oscillator.
Rneg = the real part of the impedance represented by the oscillator.
Mathematically, Rneg is a negative resistance. It represents a circuit that supplies power rather than dissipating power, for example, an amplifier. Consequently, a simple interpretation is that the amplifier must have enough gain to compensate for the losses represented by the crystal and load capacitance. The concept of negative resistance is important to crystal oscillator design and will be revisited later in this app note.
The TCAN455x clock circuit contains three main blocks, an Amplifier and Bias Control block, a Filter and Comparator block, and a Clock Input Detection block as shown in Figure 1-1. A Comparator is used to compare the voltage difference between the OSC1 and OSC2 pins and generate the Clock Output signal used by the device when either a quartz crystal or single-ended clock input is used. The positive input of the comparator is connected to the OSC1 pin, and the negative input is connected to the OSC2 pin. When a single-ended clock is used, the clock signal is applied to the positive input of the comparator through the OSC1 pin, and the negative input of the comparator is held low by connecting the OSC2 pin to ground.
The Amplifier and Bias Control block provides the source current needed to start and sustain the crystal oscillation through the OSC1 pin when a quartz crystal is used, but it must be disabled when a single-ended clock input is used instead of a crystal. This is handled by the Clock Input Detection block that monitors the voltage level on the OSC2 pin and disables the Amplifier block if the voltage is below the detection threshold which is typically between 90mV to 150mV, such as when the pin is connected to ground. If the OSC2 pin is not connected to ground, the current supplied by the Amplifier and Bias block through the crystal will ideally keep the minimum voltage level of the oscillation waveform above 400mV and includes a peak detector circuit that will sense the oscillation envelope formed by the voltage difference between the OSC1 and OSC2 pins.
The crystal oscillator transconductance amplifier adjusts the amplifier bias current to maintain a consistent and stable oscillation when the voltage amplitude of the OSC1 and OSC2 waveforms are nominally 1 Vpp for each of the individual OSC1 and OSC2 signals, or 2 Vpp between the differential OSC1 and OSC2 signal resulting from their 180° phase shift. However, the actual voltage levels will depend on the total load connected to the TCAN455x oscillator circuit.
When the total external load on the amplifier created by the reactance of the load capacitance and the crystal equivalent series resistance is too small, the amplifier's minimum output current may cause the oscillation voltage amplitude levels to become too large by allowing too much power to flow through the crystal. If the voltage amplitude on the OSC2 pin becomes too large, the minimum peak voltage level of the signal could drop below the single-ended clock input detection threshold causing the amplifier and bias block to become disabled and stop the oscillation. When the external load is configured properly, the amplifier will be able to adjust the bias current to maintain a smaller voltage amplitude level in the nominal range and ensure the single-ended clock detection circuit will not disable the amplifier and bias control block.
Establishing the proper balance in the oscillation circuit is critical to stable reliable operation, preventing mechanical damage to the crystal, and guarantee several other factors not previously discussed. Ensuring the frequency of oscillation and the gain in the transconductance amplifier has enough margin to create the negative resistance needed to reliably establish the crystal oscillation must also be considered when selecting the values of the components used in the circuit. The remainder of this document will discuss how to avoid unreliable operation and determine the proper component values needed to meet all parametric concerns through a combination of measurements and calculations.
Common schematic representations of the Basic Pierce Oscillator circuit are shown in the following figure with the key components identified.
Without a TCAN455x device, crystal, and load capacitors mounted on the board, measure the parasitic capacitance between the crystal footprint pads. If series resistors are used, include those on the board when making the measurement. This becomes the PCB stray capacitance that will be used in calculations CPCB_Stray.
The TCAN455x OSC1 Output Pin Capacitance Cout is typically 10 pF
The TCAN455x OSC2 Input Pin Capacitance Cin is typically 9 pF
Calculate the load capacitance presented to the crystal by the following formula:
Where the OSC1 pin capacitance Cout is in parallel with the CL1 external load capacitance since they are both with respect to ground on the amplifier output side of the crystal and therefore added together.
Where the OSC2 pin capacitance Cin is in parallel with the CL2 external load capacitance since they are both with respect to ground on the amplifier input side of the crystal and therefore added together.
Where the capacitance on both sides of the crystal are in series with each other relative to the crystal due to the common connection through the ground plane. Therefore they are calculated as capacitance in series.
Where the parasitic capacitance of the PCB between the OSC1 and OSC2 pins is in parallel with the capacitance of the components and is therefore added to component capacitance.
Adjust the value of the external capacitors CL1 and CL2 to achieve a total load capacitance CLoad of the recommended value specified in the crystal data sheet.