SLLA628 September 2023 THVD1424
The first step in the process is understanding what requirements the system needs to meet beyond the standard RS-485 requirements. Well defined requirements are vital for efficient and accurate IC selection. Using the variable considerations from earlier in the note the next step is to take a brief look into how requirements impact system definition. It is also important that the designer maintains which requirements are needs (specification needed for proper system operation) versus what requirements are wants (specification that provides some technical or some other pragmatic benefit but aren’t required for proper system operation) as this will help open all possible options.