SLLA628 September 2023 THVD1424
A RS-485 compliant transmitter has a few key requirements to be compliant with the standard – while this is not an exhaustive list – these tend to be the most critical across applications. The first is the output differential voltage magnitude – which is typically denoted |VOD| - which requires the magnitude of the driver to be a minimum of 1.5 V across a 54 Ω load – which is intended to show that the transmitter can drive 32 Unit Loads in Parallel with two 120 Ω termination resistors. It needs to be able to withstand an input common mode range of -7 V to 12 V – but this range can be expanded. In case of bus contention, two transmitters communicating at the same time, or a direct short to a voltage supply from a differential bus pin, or a short between differential bus pins the driver must limit the current magnitude to 250mA – this is typically denoted IOS. Finally, a more variable requirement, that of maximum differential transition time - which states that the transition time can be no more than a third of the bit time of the incoming signal.