SLLA632 March 2024 ALM2402-Q1 , DRV8243-Q1 , DRV8906-Q1 , LM74700-Q1 , MSPM0G3507-Q1 , TLIN1431-Q1 , TPS1HB08-Q1
The familiar automotive side mirror has evolved from a simple reflective glass to a highly capable subsystem. Side mirrors can provide the driver with not just a rearward view, but also with information about vehicles in your blind spot, automatic dimming when an overtaking vehicle's headlights are too bright, heat to remove ice or fog, and signals to alert other drivers when your car is making a turn. This application brief discusses the requirements and designs for controlling all these features.
In many cases, the mirror functions can be managed as part of a door module, which can also control the power window, locks, and options such as pop-out handles. In other cases, a separate mirror module can manage the mirror functions. Our design discussed in the following focuses on this second type of partition. Figure 1 illustrates some of the many features that can be found in a full-featured automotive side mirror.
Texas Instruments has designs to help designers implement all these functions. In the following paragraphs, we discuss the various sub-circuits and suggest components for implementation.
The functions of the mirror require power from the vehicle power system, typically a 12-V source, and connection to the vehicle network, usually CAN or LIN. In our design, the system basis chip (SBC) TLIN1431-Q1 provides the LIN transceiver connection to the network, as well as a voltage regulator to convert from the 12-V automotive supply to a 3.3V voltage for the microcontroller (MCU) and analog signals. This device also includes a watchdog function to monitor the MCU and provides a reset if needed. An LM74700-Q1 smart diode protects the module against reverse battery conditions.
The microcontroller (MCU) coordinates and controls the functions of the side mirror. The MCU processes messages from the vehicle network, typically either LIN or CAN, and controls the motors, heater and LEDs in response to network commands or button pushes from the vehicle driver.
The MCU monitors the operation of each of the functions, and takes action if any faults are detected, such as overload conditions, excessive temperatures, or voltage supply faults. Our design uses an MSPM0 Arm® Cortex®-M0+ microcontroller to manage all the side mirror functions. For designs where the vehicle network is CAN, the MSPM0G3507 integrates a CAN controller into the MCU. For designs where LIN is the network connection, the MSPM0L1305 can be a good choice. In addition to the typical digital features, these MCUs also integrated useful analog components, including op amps and comparators. This simplifies signal conditioning of sensor inputs and diagnostics, for example.
The horizontal (X) and vertical (Y) adjustment of the mirror position typically use small brushed DC motors, with typical current less than 1A. In our design, three half-bridges of the DRV8906-Q1 drive these two motors, allowing movement in either direction on the X or Y axis. If pulse-width modulation is desired to control the speed of the motion, the DRV8906-Q1 has integrated PWM generators, settable by the MCU through the serial peripheral interface (SPI).
In tight parking spaces, every inch of width counts. Folding side mirrors can reduce the width of the car by several inches on each side, preventing damage from scraping on obstacles and allowing more room to exit and enter the car. When motorized, this feature is typically implemented with a brushed DC motor, requiring a simple full-bridge drive, with a current of a few amps. In our design, we use the DRV8243-Q1 fully-integrated motor driver, which can drive up to 12 amps. Since the mirror fold has a limited range of motion, typically about 90 degrees, we want to stop driving when the mirror reaches either the fully open or fully closed position. The DRV8243-Q1 has an output signal proportional to the motor current, so we can determine the end-of-travel when the motor current increases as it reaches a stall point. We can also set an adjustable current limit, so the motor torque does not cause binding.
Snow and ice can obscure the mirror, so a resistive heating element is built into the back surface of many side mirrors, allowing the driver to defrost the mirror without manually cleaning it. Depending on the size of the mirror, the heater may require a few amps of current. Our design uses a TPS1HB08-Q1 high-side switch to supply the heater current. This device has an RDS(ON) of 8 milliOhms for driving currents up to 10A. An adjustable current limit and comprehensive diagnostics ensure reliable operation.
Electrochromic tinting allows a mirror to change the reflectivity to reduce glare when needed. When no voltage is applied, the electrochromic coating is clear, allowing normal reflectivity. When a voltage is applied, the coating darkens, reducing the amount of reflected light. The electrical properties of the coating require a relatively large charge to change the tint, with a larger current required for a larger surface area. Typically the tint can be set in a continuous range, from completely transparent to very dark, depending on the applied voltage. In our design, an ALM2402-Q1 power op amp is used to supply the current needed along with the continuously-variable voltage in response to a DAC output from the MCU.
In addition to a rearward view, the side mirror has taken on additional functions to provide information to the driver and to other vehicles. Turn indicators on the outer edge of the mirror increase the visibility of that signal beyond the traditional front and rear blinkers. A blind spot warning indicator is provided to shine through the mirror surface and alert the driver to surrounding traffic. A puddle light shining downwards from the bottom of the mirror stalk lights the ground near the door, assisting the driver approaching the parked car. Other illumination might include front-facing spotlights and running lights or trim illumination. Our design uses three of the DRV8906-Q1 channels to provide high-side drive for these LEDs. If more channels are needed, devices with up to 12 channels are available in that same footprint. On-chip PWM generators are settable through the SPI interface for any desired level of brightness for each channel.
Figure 2 shows an implementation of the side mirror module block diagram of Figure 1. This board includes all the features described, as well as buttons, connectors, and test points for bench evaluation of the circuits. In a production mirror module, these extra components are not needed, reducing the size of the board.
Automotive side mirrors have evolved to have many features to enhance safety and convenience for drivers and passengers. Texas Instruments has a broad portfolio of devices available for these functions, and our example gives designers a head-start in understanding and choosing designs for side mirror applications.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2024, Texas Instruments Incorporated