SLLA641 July 2024 TAA5212 , TAC5112 , TAC5212
The following are two different Microphones used in this application examples; POM-2242P-C33-R and POM-2730L-HD-R. Using the microphone information from the data sheet, tests are run on converter devices that has PGA and TAX5XXX converter which has the new ADC front-end architecture.
In each of the microphone case, the following test conditions were run:
From each of the test cases above, the performance is compared between the 2 converter devices.
The device we use with PGA integrated is TLV320ADC6120; a high performance audio analog-to-digital converter (ADC) with 123dB Dynamic Range with DRE enable and 113dB with DRE disabled in the AC-Coupled differential input and TAA5212; a low-power high-performance stereo audio ADC with 118dB dynamic range in the new ADC front-end architecture.