The TUSB564-Q1 is an automotive USB 3.1 5-Gbps Alt-mode redriver designed to enable DisplayPort Alt-mode over USB-C. This device multiplexes between USB and DisplayPort signals sent over the USB-C interface in a DisplayPort sink application. USB and DisplayPort signal amplitudes attenuate through a typical FR4 channel, placing limitations on system trace length at 5Gbps and higher data rates. A longer channel with large attenuation results in signal integrity issues at a USB or DisplayPort receiver. The TUSB564-Q1 is used to eliminate or minimize the attenuation effects of the channel to produce a compatible eye at the device receiver. Attenuation is minimized by applying receiver equalization to compensate for cable and board loss due to intersymbol interference (ISI) and insertion loss. The TUSB564-Q1 is configurable with 16 receiver equalization settings for USB signals and 16 equalization settings for Displayport signals.
Equalization Selection
The TUSB564-Q1 used in a device application enables the system to pass USB 3.1 Gen 1 transmitter and receiver compliance, as well as DisplayPort receiver compliance. The TUSB564-Q1 recovers incoming data by applying equalization that compensates for channel loss, typical FR4 channel loss is provided in Table 1. Base the equalization on the amount of insertion loss of the channel before the TUSB564-Q1 receiver (Pre-Channel). The EQ values of the USB TX, USB RX, and DisplayPort RX are set independently. The equalization selection is configured through the EQ, SSEQ, and DPEQ pins. The USB equalization values available for the TUSB564-Q1 are listed in Table 2.
FR4 PCB Trace Length (inches) | Loss at 2.5GHz (dB) |
---|---|
1 | 0.5 |
2 | 1 |
3 | 1.5 |
4 | 2 |
5 | 2.5 |
6 | 2.9 |
7 | 3.4 |
8 | 3.9 |
9 | 4.4 |
10 | 4.9 |
11 | 5.4 |
12 | 5.9 |
13 | 6.4 |
14 | 6.9 |
EQ Setting # | USB 3.1 Upstream Facing Ports | USB 3.1 Downstream Facing Ports | ||||
---|---|---|---|---|---|---|
EQ1 | EQ0 | EQ Gain at 2.5GHz (dB) | SSEQ1 | SSEQ0 | EQ Gain at 2.5GHz (dB) | |
0 | 0 | 0 | -0.7 | 0 | 0 | -0.9 |
1 | 0 | R | 1.8 | 0 | R | 0.2 |
2 | 0 | F | 2.7 | 0 | F | 1.1 |
3 | 0 | 1 | 3.7 | 0 | 1 | 2.2 |
4 | R | 0 | 4.6 | R | 0 | 3.0 |
5 | R | R | 5.5 | R | R | 4.0 |
6 | R | F | 6.3 | R | F | 4.8 |
7 | R | 1 | 7.0 | R | 1 | 5.6 |
8 | F | 0 | 7.8 | F | 0 | 6.4 |
9 | F | R | 8.5 | F | R | 7.0 |
10 | F | F | 9.1 | F | F | 7.6 |
11 | F | 1 | 9.7 | F | 1 | 8.2 |
12 | 1 | 0 | 10.1 | 1 | 0 | 8.7 |
13 | 1 | R | 10.7 | 1 | R | 9.2 |
14 | 1 | F | 11.1 | 1 | F | 9.7 |
15 | 1 | 1 | 11.6 | 1 | 1 | 10.2 |
AUX Snoop
For DisplayPort Alt-mode applications, the TUSB564-Q1 snoops the AUX lines by default to determine lane count when passing video signals. AUX snooping helps to conserve power when not all four data lanes are used for DisplayPort data. Deactivate AUX snooping when the TUSB564-Q1 is in I2C mode by writing a "1" in the AUX_SNOOP_DISABLE register. While AUX snooping is inactive, manually enable the DisplayPort lanes through the DPx_DISABLE registers where x = 0, 1, 2, or 3.
Following the layout guidelines listed in this document enables the TUSB564-Q1 to recover a signal from a USB device up to a typical 14-inch FR4 trace. In addition, the FR4 trace from the TUSB564-Q1 to the USB connector can be up to 5 inches. These recommended maximum trace lengths assumes the device provides -3 dB of de-emphasis and has a compliant receiver that recovers the 20dB loss budgeted by the USBIF for a Type-C cable and the host or device. Maximum trace lengths are extendable by adjusting the equalization, de-emphasis, and VOD settings of a device; best settings are determined in conjunction by the user and the device manufacturer. Conversely, if a device is unable to recover the signal with the amount of budgeted loss set by the USBIF, then concessions are required in the system design, such as placement of the device.
Figure 2 provides an example configuration of a device system using a USB3.1 Gen 1 device operating at 5Gbps and a DisplayPort 1.4 sink operating at 8.1Gbps with the TUSB564-Q1.
Using the given trace lengths in this example, the method to select the equalization values for SSTX and RX1/2 is to select the closest EQ gain available to match the trace loss and additional loss through the connector, components, and device package:
Please note that other factors such as the layout quality, device transmitter and receiver quality require adjusting the EQ settings for best performance. Use the above method to select the initial configuration values based on system board trace lengths.
Use the following layout guidelines in routing the high-speed USB signals to and from the TUSB564-Q1.
GND Stitching
The entirety of any high-speed signal trace must maintain the same GND reference plane from origination to termination. If the same GND reference plane is not maintained, via-stitch the GND planes together to establish continuous grounding and uniform impedance. Place these stitching vias symmetrically within 200-mils (center-to-center, closer is better) of the signal transition vias. See Figure 3 below for an example of GND stitching vias.
AC Coupling and Resistor Placement
When placing AC-Coupling capacitors, the maximum component size is 0402 . During layout, on the host or device channel, place the AC-Coupling capacitors equidistant to the device and the TUSB564-Q1. On the connector to TUSB564-Q1 channel, place the AC Coupling caps close to the TUSB564-Q1 with symmetrical placement to establish top signal quality and to minimize reflections. Place the optional pull-down resistors so that the pad of the resistor shares the high-speed trace to minimize the presence of a stub. See Figure 4 for an example of the optimal AC Coupling capacitor layout symmetry.