SLLA655 September   2024 TUSB1044

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Getting Started
  5. 2Low Level Page
  6. 3High Level Page
  7. 4References

Low Level Page

  1. When the device is selected, the complete register map appears in the table below.
    TUSB1044
  2. Click the Read All button to read the configuration of the entire device. Alternately, select a specific register and click the Read Register button to update the target register quicker. The current address field automatically updates with the highlighted register.
    TUSB1044
  3. To write to the selected register, check or deselect the boxes in the Register Data field. You can also manually enter a hex value into the Data field. Click the Write Register button to complete the update, then click the Read Register button to verify that the change was made. Note the Field Description table describes the function of each bit in the highlighted register
  4. Use the Save Config and Load Config buttons to save the current configuration in a .cfg file, and load the file back as needed. Click the Reset Device button to reset every setting to the default.