SLLSEP9I september 2015 – august 2023 SN6505A , SN6505B
PRODUCTION DATA
The following application circuits are shown for a 3.3 V input supply commonly taken from the local, regulated microcontroller supply. For 5 V input voltages requiring different turn ratios refer to the transformer manufacturers and their web sites listed in Table 9-4.
MANUFACTURER | MORE INFORMATION |
---|---|
Coilcraft Inc. | http://www.coilcraft.com |
Halo-Electronics Inc. | http://www.haloelectronics.com |
Murata Power Solutions | http://www.murata-ps.com |
Wurth Electronics Midcom Inc | http://www.midcom-inc.com |