SLLSEX2F December 2016 – April 2024 TDP158
PRODUCTION DATA
When OE is low, control signal inputs are ignored; the HDMI inputs and outputs are high impedance. It is critical to transition the OE from a low level to high after the VCC supply has reached the minimum recommended operating voltage. This is achieved by a control signal to the OE input, or by an external capacitor connected between OE and GND. To properly reset the TDP158, the OE pin must be de-asserted for at least 100 μs before being asserted. When OE is re-asserted the TDP158 must be reprogrammed if it was programmed by I2C and not pin strapping. When implementing the external capacitor, the size of the external capacitor depends on the power up ramp of the VCC supply, where a slower ramp-up results in a larger value external capacitor. Refer to the latest reference schematic for TDP158; consider approximately 0.1 µF capacitor as a reasonable first estimate for the size of the external capacitor. Both OE implementations are shown in Figure 7-1 and Figure 7-2.