SLLSF80B October 2019 – March 2022 TCAN1144-Q1 , TCAN1145-Q1 , TCAN1146-Q1
PRODUCTION DATA
Figure 11-7 shows the behavior of the INH pin during a brownout event. Brownout is when VSUP is ≤ UVSUP but > POR state. The RXD pin has an internal pull-up resister that is active during this event and will pull up the RXD pin output to the voltage level of VIO.
When the TCAN114x has a UVSUP event, the CAN bus will be biased to ground.