The following procedure should be
followed to write data to TUSB1104 I2C registers (refer to
Figure 7-2):
- The controller initiates a write operation by generating a
start condition (S), followed by the TUSB1104 7-bit address and
a zero-value “W/R” bit to indicate a write cycle.
- The TUSB1104 acknowledges the address
cycle.
- The controller presents the register offset within TUSB1104 to be written, consisting of one byte of data,
MSB-first.
- The TUSB1104 acknowledges the sub-address
cycle.
- The controller presents the first byte of data to be written to
the I2C register.
- The TUSB1104 acknowledges the byte
transfer.
- The controller may continue presenting additional bytes of data
to be written, with each byte transfer completing with an acknowledge from
the TUSB1104.
- The controller terminates the write operation by generating a
stop condition (P).
The following procedure should be
followed to read the TUSB1104 I2C registers without a
repeated Start (refer Figure 7-3).
- The controller initiates a read operation by generating a start
condition (S), followed by the TUSB1104 7-bit address and a
zero-value “W/R” bit to indicate a read cycle.
- The TUSB1104 acknowledges the 7-bit address
cycle.
- Following the acknowledge the controller continues sending
clock.
- The TUSB1104 transmit the contents of the
memory registers MSB-first starting at register 00h or last read register
offset+1. If a write to the I2C register occurred prior to the
read, then the TUSB1104 shall start at the register offset
specified in the write.
- The TUSB1104 waits for either an acknowledge
(ACK) or a not-acknowledge (NACK) from the controller after each byte transfer;
the I2C controller acknowledges reception of each data byte
transfer.
- If an ACK is received, the TUSB1104 transmits
the next byte of data as long as controller provides the clock. If a NAK is
received, the TUSB1104 stops providing data and waits for a
stop condition (P).
- The controller terminates the write operation by generating a
stop condition (P).
The following procedure should be
followed to read the TUSB1104 I2C registers with a repeated
Start (refer Figure 7-4).
- The controller initiates a read operation by generating a start
condition (S), followed by the TUSB1104 7-bit address and a
zero-value “W/R” bit to indicate a write cycle.
- The TUSB1104 acknowledges the 7-bit address
cycle.
- The controller presents the register offset within TUSB1104 to be written, consisting of one byte of data,
MSB-first.
- The TUSB1104 acknowledges the register offset
cycle.
- The controller presents a repeated start condition (Sr).
- The controller initiates a read operation by generating a start
condition (S), followed by the TUSB1104 7-bit address and a
one-value “W/R” bit to indicate a read cycle.
- The TUSB1104 acknowledges the 7-bit address
cycle.
- The TUSB1104 transmit the contents of the
memory registers MSB-first starting at the register offset.
- The TUSB1104 shall wait for either an
acknowledge (ACK) or a not-acknowledge (NACK) from the controller after each
byte transfer; the I2C controller acknowledges reception of each data
byte transfer.
- If an ACK is received, the TUSB1104 transmits
the next byte of data as long as controller provides the clock. If a NAK is
received, the TUSB1104 stops providing data and waits for a
stop condition (P).
- The controller terminates the read operation by generating a
stop condition (P).
The following procedure should be
followed for setting a starting sub-address for I2C reads (refer to Figure 7-5).
- The controller initiates a write operation by generating a
start condition (S), followed by the TUSB1104 7-bit address and
a zero-value “W/R” bit to indicate a write cycle.
- The TUSB1104 acknowledges the address
cycle.
- The controller presents the register offset within TUSB1104 to be written, consisting of one byte of data,
MSB-first.
- The TUSB1104 acknowledges the register offset
cycle.
- The controller terminates the write operation by generating a
stop condition (P).
Note:
After initial power-up, if no
register offset is included for the read procedure (refer to Figure 7-3), then reads
start at register offset 00h and continue byte by byte through the registers
until the I2C controller terminates the read operation. During a read
operation, the TUSB1104 auto-increments the I2C internal
register address of the last byte transferred independent of whether or not an
ACK was received from the I2C controller.