The following instructions assume
the EVM is configured for pin-strap mode and is powered from barrel jack. To
start the EVM, do the following:
- Insert the +5 V
DC power source into the barrel jack. Turn on SW2.
- If using external
I2C configuration instead of pin-straps, then please
configure TMDS1204 at this step.
- Insert an HDMI
source using a standard HDMI cable into P1 (HDMI
receptacle).
- Insert an HDMI
video sink into P2 (HDMI receptacle) using a standard HDMI
cable.
- Video output on
HDMI sink should be observed.