3.4 Step-by-Step Instructions for Operation and Troubleshooting
After the user has acquired the
necessary hardware and software, follow these steps to operate the USB interface
adapter:
Plug in the USB cable to both the
PC and the USB interface adapter and wait for the green LED to illuminate. Troubleshooting: If the green LED does not
illuminate after 30 seconds, check to ensure the USB cable is securely
connected. If the connection is secure, try a different USB port. If a different
USB port does not solve the problem, try to reboot the computer. If rebooting
the computer does not fix the problem, try a different USB cable. If trying
different USB cable does not solve the problem, contact TI technical support for
help.
Plug in the 10-pin ribbon cable
to both the USB interface adapter and an I2C device board. Make sure
that the notch on the ribbon-cable connector matches the keyhole of the socket
in the enclosure.
Power up the I2C
board. Note that the default I2C speed is set at 100 kHz and the
default pullups for I2C data and clock lines are set at 2.2 kΩ.
Open the Fusion Digital Power
designer tool and follow the instructions for the GUI. Troubleshooting: If the I2C
target board cannot talk with the USB interface adapter, first check to ensure
the 10-pin ribbon cable has been securely connected. If the ribbon cable has
been securely connected, check the I2C communication speed and the
pullups for I2C data and clock lines suitable for the application. If
not, modify the I2C communication speed and the pullups accordingly.
If this still does not solve the problem, contact the manufacturer of the
I2C targeted board for help.