USB Type-C is a trademark of USB Implementers Forum.
All trademarks are the property of their respective owners.
The TUSB1142EVM is a PCB created to help for customers to evaluate the TUSB1142. The EVM has a USB Type-B receptacle and a USB Type-C receptacle. The user of the EVM can insert a USB 3 Micro-B cable to the TUSB1142EVM board then connect to a USB 3 Gen 1/2 motherboard or system with a USB Type-A receptacle. The user can insert a USB device directly or thru a USB Type-C cable into the receptacle side of the EVM board.