This document is provided with the MCF8315 customer evaluation module (EVM) as a supplement to the MCF8315 data sheet (MCF8315A Three-Phase Sensorless-FOC BLDC Motor Driver). This User's Guide details the hardware implementation of the EVM and how to setup and power the board.
LaunchPad™ is a trademark of Texas Instruments.
All trademarks are the property of their respective owners.
Observe the following cautions and warnings as printed on the EVM board.
HOT SURFACE: |
![]() |
Caution Hot Surface! Contact may cause burns. Do not touch. Please take the proper precautions when operating. |
The MCF8315 is a 4.5-V to 35-V, 5-A peak integrated three-phase gate driver IC with sensorless field-oriented control for motor drive applications. It provides three accurately trimmed and temperature compensated half-bridge MOSFETS, gate drivers, charge pump, current sense amplifier, linear regulator for the external load and adjustable buck regulator. The I2C interface variant (MCF8315) also provides a standard I2C interface for configuring the various device settings and reading fault diagnostic information through an external controller.
The MCF8315EVM includes an onboard FTDI chip to convert USB communication from the micro-USB connector into UART and an onboard MSP430FR2355 MCU to interface with the MCF8315. It can also provide SPI communication for the SPI variant of the MCF8315 device. There are many user-selectable jumpers, resistors, connectors, and test points to evaluate many features of the device and configure device-specific settings.
This document serves as a startup guide to supplement the MCF8315EVM. It is intended for engineers to design, implement, and validate reference hardware for the MCF8315 device.
The MCF8315EVM requires a power supply source, which has a recommended operating range from a 4.5-V to 35-V. To setup and power the EVM, follow the sequence below: