SLLU363 may 2023 MCF8315A
MCF8315A provides four options to configure the input speed command.
Configure the speed input [SPEED_MODE] register to select the desired speed input mode.
If PWM input on SPEED pin is chosen as the speed input, configure [SPEED_RANGE_SEL] to select the PWM frequency range.
If Frequency input on SPEED pin is chosen as the speed input, configure [INPUT_MAXIMUM_FREQ] to select the maximum PWM frequency. For example, if 10 kHz is chosen as maximum PWM frequency, 10 kHz PWM signal on SPEED pin corresponds to 100% speed command.
Note that even when [SPEED_MODE] is configured as Analog input, PWM input, or Frequency input, the [OVERRIDE] toggle can still be used to override the speed input using the in the I2C Control Section in GUI.