SLLU363 may 2023 MCF8315A
Acoustics is audible noise contributed by motor commutation and harmonic frequencies in motor drives. Stator excitation in motor drivers can generate mechanical resonance at audible frequency ranges leading to audible noise. Improving acoustic performance is important for applications that require quiet operation. Any distortion in phase current can translate to audible noise. Phase current distortion can be due to dead time, PWM modulation scheme or low MOSFET slew rate.
Step 1: Configure PWM Modulation scheme [PWM_MOD] to “Continuous Space Vector Modulation”.
In Continuous Space vector modulation, phase current waveform shaping is better but the MOSFET switching losses is higher.
In Discontinuous Space vector modulation, MOSFET switching losses are lower. However, we can expect phase current distortion for low inductance motors.
Step 2: Enable Dead time compensation [DEADTIME_COMP_EN]
Figure 3-1 shows the phase current waveform when dead time compensation is disabled. Fundamental frequency of phase current is 40 Hz. Fast Fourier transform (FFT) of phase current plot shows harmonics at 160 Hz and 220 Hz. Figure 3-2 shows the phase current waveform when dead time compensation is enabled. Phase current looks more sinusoidal and the FFT of phase current plot does not have any harmonics.