SLLU373 November 2023
This document is provided with the MCF8329 customer evaluation module (EVM) as a supplement to the MCF8329 data sheet. This user's guide details the hardware setup instructions, GUI installation, and usage instructions.
Hot surface temperature
The EVM can have high surface temperatures marked by the FIRE triangular symbol on the EVM. Avoid toughing the marked hot surface are when driving high currents to prevent potential burn damage.