SLLU373 November 2023
The MCF8329EVM includes a USB-to-UART interface, using a MSP430FR2355 microcontroller, that serves as a communication bridge between a host PC and the MCF8329 device for configuring various device settings and reading fault diagnostic information.
The MCF8329EVM is supported on the Motor Studio GUI which can be used to configure the MCF8329 though this communication interface. The Motor Studio GUI simplifies the tuning process of the MCF8329 by offering guided tuning instructions, a virtual oscilloscope for real-time variable monitoring, and more. The latest version of the Motor Studio GUI can be downloaded on ti.com.
By default, the onboard MSP430 microcontroller already contains the firmware needed to communicate with the Motor Studio GUI. If there is a firmware update or the GUI does not connect to the EVM, then the user must flash the firmware code into the MSP430 by following the steps outlined in Section 3.4.
Flashing the firmware code onto the MSP430 requires an integrated development environment (IDE) and an eZ-FET Debug Probe. The following example uses the Code Composer Studio™(CCS) IDE and the MSP-EXP430FR2355 LaunchPad™ Development Kit to provide the eZ-FET Debug Probe.