This fault gets triggered when the
phase current is below the no motor lock threshold for 500ms during open loop. When
this fault gets triggered, use the following recommendations:
- Make sure the motor phases are
securely connected to the OUTA, OUTB, and OUTC test points or the connector
block J11.
- If the fault persists, set the no
motor lock current threshold [NO_MTR_THR] to 5%.
- For low inductance motors,
increase PWM switching frequency [PWM_FREQ_OUT].
Note: The MCF8329A might trigger loss of
sync [LOSS_OF_SYNC] when motor phases are disconnected while the motor is
spinning.