SLLU374 November 2024 MCF8329A
Once all the other settings covered in the Section 4.1 section are set, the MPET algorithm within the MCF8329A can be used to measure the BEMF constant and speed loop gains needed to spin the motor in closed loop. Before running MPET, go to the MPET page and check that the IPD and open loop current limits are set according to the instructions in Section 4.1.3. Next, enable the Measure Motor BEMF Constant and Measure Motor Mechanical Parameter switches and click the Run MPET button. The motor should begin to spin. After the motor stops spinning, MPET has completed measuring. Click the Write MPET Results To Shadow Registers button to use the results measured by MPET.