SLLU383 October 2024
The MCF8329RRYEVM includes a MSP430FR2355 low-power MCU, shown in Figure 2-5, to communicate via I2C with the MCF8329 IC.
To program the MSP430FR2355, an external MSP430 FET programmer must be connected to the Spy-Bi-Wire (SBW) interface connector J7. Many MSP430 LaunchPads™ provide an onboard eZ-FET Debug Probe that can be jumper-wired to the MCF8329RRYEVM to flash the firmware into the onboard MSP430FR2355 microcontroller.
The Reset (RST) button at any time to restart the MCU program. Two active-low LEDs, D13 and D14, can be used for debug purposes as well.
The 32-pin shunt jumper bridge J9 ties all signals between the microcontroller and MCF8329 IC. These jumpers can be inserted or removed as needed to isolate the microcontroller from the gate driver. This allows for microcontroller signal debugging or using the MCF8329RRYEVM as a standalone gate driver with an external microcontroller.