The Motor Studio GUI can be used to interface with and configure the MCF8315.
- Connect the MCF8315PWPEVM as described in Section 2.2.
- Download the latest version of the Motor Studio GUI.
- Once the Motor Studio GUI is installed, run the Motor Studio GUI application.
- Click the red Setup Now button under Hardware Setup on the bottom right side of the window.
- After setting up the hardware settings of the MCF8315PWPEVM, click on the Quick Spin option to begin configuring the device.
Once the GUI is loaded, follow the Quick Spin page of the GUI to spin up the motor.