SLOA011B January   2018  – July 2021 LF347 , LF353 , LM348 , MC1458 , TL022 , TL061 , TL062 , TL071 , TL072 , UA741

 

  1. 1Introduction
    1. 1.1 Amplifier Basics
    2. 1.2 Ideal Op Amp Model
  2. 2Non-Inverting Amplifier
    1. 2.1 Closed Loop Concepts and Simplifications
  3. 3Inverting Amplifier
    1. 3.1 Closed Loop Concepts and Simplifications
  4. 4Simplified Op Amp Circuit Diagram
    1. 4.1 Input Stage
    2. 4.2 Second Stage
    3. 4.3 Output Stage
  5. 5Op Amp Specifications
    1. 5.1  Absolute Maximum Ratings and Recommended Operating Condition
    2. 5.2  Input Offset Voltage
    3. 5.3  Input Current
    4. 5.4  Input Common Mode Voltage Range
    5. 5.5  Differential Input Voltage Range
    6. 5.6  Maximum Output Voltage Swing
    7. 5.7  Large Signal Differential Voltage Amplification
    8. 5.8  Input Parasitic Elements
      1. 5.8.1 Input Capacitance
      2. 5.8.2 Input Resistance
    9. 5.9  Output Impedance
    10. 5.10 Common-Mode Rejection Ratio
    11. 5.11 Supply Voltage Rejection Ratio
    12. 5.12 Supply Current
    13. 5.13 Slew Rate at Unity Gain
    14. 5.14 Equivalent Input Noise
    15. 5.15 Total Harmonic Distortion Plus Noise
    16. 5.16 Unity-Gain Bandwidth and Phase Margin
    17. 5.17 Settling Time
  6. 6References
  7. 7Glossary
  8. 8Revision History

Ideal Op Amp Model

The Thevenin amplifier model shown in Figure 1-1 is redrawn in Figure 1-2 showing standard op amp notation. An op amp is a differential to single-ended amplifier. It amplifies the voltage difference, Vd = Vp - Vn, on the input port and produces a voltage, Vo, on the output port that is referenced to ground.

GUID-C99C6061-BB74-4527-A5E1-AFE12BABD441-low.gifFigure 1-2 Standard Op Amp Notation

We still have the loading effects at the input and output ports as noted above. The ideal op amp model was derived to simplify circuit calculations and is commonly used by engineers in first-order approximation calculations. The ideal model makes three simplifying assumptions:

  • Gain is infinite
    Equation 1. a = ∞
  • Input resistance is infinite
    Equation 2. Ri = ∞
  • Output resistance is zero
    Equation 3. Ro = 0

Applying these assumptions to Figure 1-2 results in the ideal op amp model shown in Figure 1-3.

GUID-7464A55A-CDC8-48DF-95ED-FFC1CDD02EE0-low.gifFigure 1-3 Ideal Op Amp Model

Other simplifications can be derived using the ideal op amp model:

Equation 4. → In = Ip = 0

Because Ri = ∞, we assume In = Ip = 0. There is no loading effect at the input.

Equation 5. → Vo = a Vd

Because Ro = 0 there is no loading effect at the output.

Equation 6. → Vd = 0

If the op amp is in linear operation, V0 must be a finite voltage. By definition Vo = Vd × a. Rearranging, Vd = Vo / a . Since a = ∞, Vd = Vo / ∞ = 0. This is the basis of the virtual short concept.

Equation 7. Common mode gain = 0

The ideal voltage source driving the output port depends only on the voltage difference across its input port. It rejects any voltage common to Vn and Vp.

Equation 8. Bandwidth = ∞
Equation 9. Slew Rate = ∞

No frequency dependencies are assumed.

Equation 10. Drift = 0

There are no changes in performance over time, temperature, humidity, power supply variations, etc.