SLOA011B January 2018 – July 2021 LF347 , LF353 , LM348 , MC1458 , TL022 , TL061 , TL062 , TL071 , TL072 , UA741
Normally there is a voltage that is common to the inputs of the op amp. If this common mode voltage gets too high or too low, the inputs will shut down and proper operation ceases. The common mode input voltage range, VICR, specifies the range over which normal operation is guaranteed.
Figure 5-2 illustrates the positive input voltage limit using the simplified op amp diagram of Figure 4-1. When VIN is higher than VCC - 0.9 V, the input transistors and the current source will begin to shut down.
Figure 5-3 illustrates the negative input voltage limit using the simplified op amp diagram of Figure 4-1. When VIN is less than –VEE + 0.6 V, the current mirror (Q3 - Q4) will begin to shut down.
Structures like the one shown in the example above do not allow the common-mode input voltage to include either power supply rail. Other technologies used to construct op amp inputs offer different common-mode input voltage ranges that do include one or both power supply rails. Some examples are as follows (reference schematics can be found in the Texas Instruments’ data book, Amplifiers, Comparators, and Special Functions):