SLOA049D July 2000 – February 2023
The transfer function of a second-order low-pass filter can be expressed as a function of frequency ( ) as shown in Equation 17, the Second-Order Low-Pass Filter Standard Form.
In this equation, is the frequency variable, is the cutoff frequency, is the frequency scaling factor, and is the quality factor. Equation 17 has three regions of operation: below cutoff, in the area of cutoff, and above cutoff. For each area, Equation 17 reduces to:
With attenuation at frequencies above increasing by a power of two, the last formula describes a second-order low-pass filter.
The frequency scaling factor is used to scale the cutoff frequency of the filter so that it follows the definitions given before.