SLOA049D July 2000 – February 2023
The Butterworth polynomial requires the least work out of the three types of filters because the frequency scaling factor is always equal to one.
Referring to a table listing the zeros of the second-order Butterworth polynomial:
This is used with the factored form of the polynomial. Alternatively, the coefficients of the polynomial and can be found. The formula in Equation 19 can be confirmed:
To translate the polynomial into standard form, use the coefficient form of the polynomial in the denominator of the transfer function. The realization of a second-order low-pass Butterworth filter is made by a circuit with the following transfer function:
Equation 20 is the same as Equation 17 with and
Figure 5-1 is an example of a Second-Order Butterworth Low-Pass Filter using the Sallen-Key topology and TLV9062 created with the Filter Design Tool. This circuit has a gain of 1 V/V and a pass-band frequency at 1 kHz. The circuit was built in PSpice and then constructed and measured with a gain-phase analyzer.
Figure 5-2 and Figure 5-3 show the Butterworth low-pass filter with TLV9062 PSpice and Measured results, respectively.