SLOA059B October   2022  – March 2023 OPA2991 , TLC2654 , TLC4502 , TLE2021 , TLV2721

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2Input Offset Voltage Defined
  5. 3Cause of VOS
  6. 4VOS and Temperature Drift in the Major Device Types
    1. 4.1 Bipolar
    2. 4.2 JFET
    3. 4.3 CMOS
  7. 5Manufacturer Measurement, Trim, and Specification of VOS
    1. 5.1 Measurement
    2. 5.2 Trim
    3. 5.3 Specifications
  8. 6Impact of VOS on Circuit Design and Methods of Correction
    1. 6.1 AC Coupling
    2. 6.2 DC Feedback
    3. 6.3 Internal Calibration
  9. 7Summary
  10. 8References
  11. 9Revision History

Summary

The DC parameters represent internal errors that occur as the result of mismatches between devices and components inside the op amp. The precision of the op amp is determined by the magnitude of these errors. One of the primary DC errors is the input offset voltage (VOS) and is defined as the voltage that must be applied between the two input terminals of an op amp to obtain zero volts at the output. VOS is symbolically represented by a voltage source that is in series with either the positive or negative input terminal, that can have either negative or positive polarity, and that varies from device to device.

VOS is caused by the mismatch of the input transistors and components, primarily in the input stage of the op amp. Such errors are mostly introduced during fabrication of the silicon die, with a minor contribution from stresses placed on the die during the packaging process. These effects collectively produce a mismatch of the bias currents that flow through the input circuit, resulting in a voltage differential at the input terminals of the op amp.

There are three general manufacturing processes into which most op amps can be grouped: CMOS, JFET, and bipolar. CMOS devices typically have the lowest VOS of the three, and they have the least drift. JFET devices have the worst VOS and temperature drift. Bipolar devices have a VOS that is close to that of CMOS devices, and a low temperature drift.

All devices are tested prior to shipment to the customer to ensure their offset is below the maximum specified in the data sheet. DC parameters are measured using a servo loop and are normally trimmed during this measurement process. Devices in multiple packages often have less trim capability because of limited space available on the die. When this occurs, VOS varies between the single, dual, and quad packages. The op amps with bipolar and JFET inputs use a Zener diode trim technique to reduce the offset voltages. Op amps with CMOS inputs use a fuse-link trim network because a CMOS diode structure is not available. Laser trim is another alternative that is often used to lower VOS.

An op amp's VOS can be found in the op amp's data sheet under the input specifications table. This is done with all the error sources because the actual output created by any error source depends on the closed-loop gain (ACL) of the circuit as seen from the error source. VOS is multiplied by ACL for the non-inverting circuit to be referenced to the output. There are three major VOS specifications that may be provided for an op amp: VOS at 25°C, VOS full range, and VOS drift over temperature (ΔVOS/ΔT). The specification is fully tested and assured when the maximum or minimum values are listed. Typical specifications are not assured. Data graphs only show typical specification information.

An error budget analysis helps determine all the DC error sources in the system and the maximum contribution the design allows for each section. When the op amp or other device fails to meet the specification for VOS, they are compensated to remove or reduce the offset. Methods of reducing the effects of VOS include AC-coupling and DC feedback. In some applications, the solution is to use devices that have some form of internal or external calibration such as chopper stabilization, an auto-zero loop, or offset trim.

Audio amplifiers, communications circuits, and converters often use AC-coupling to remove VOS. DC feedback is often used in measurement systems that require precision. Many devices such as instrumentation amplifiers, data converters, codecs, processors, and CMOS chopper amplifiers and Self-Cal™ amplifiers correct the offsets internally. Most of these techniques minimize VOS only, and at only one temperature. The chopper amplifiers provide continuous correction, even over a temperature range, so they have very low drift. There are drawbacks to each method of VOS correction that must be considered for each design.