SLOA194A May 2014 – January 2022 DRV2603 , DRV2604 , DRV2604L , DRV2605 , DRV2605L , DRV2605L-Q1 , DRV2624 , DRV2625 , DRV2667
An ERM is a DC motor with an off-center mass that spins to create vibrations. When the ERM rotates, the off-center mass results in a centripetal force; this kind of centripetal force causes displacement of the motor. People perceive this displacement as a vibration. The ERM vibrates because of rotation forces so there is acceleration on two axes (X, Y, or Z axis). This creates losses in unintentional axes in some applications.
Advantages:
Disadvantages: