The Near Field Communication (NFC) market is emerging into multiple fields including medical, consumer, retail, industrial, automotive, and smart grid. Card emulation is one of the three operational modes supported by the TRF7970A. When using card emulation, the user can configure the TRF7970A to emulate a Type 4A or Type 4B tag platform. When emulating either of the tag platforms, record type definitions (RTD) can be used such as text, URI, smart poster, or V-Card. It should also be noted here that card emulation on the TRF7970A is not limited to NFC applications. Other applications could include payment systems, access control, proprietary customer systems, and other ISO 14443-4 applications. This application report describes the fundamental concepts of how card emulation is to be implemented and also how to successfully accomplish the mastery of the concept while using the TRF7970A.
The sample code described in this document can be downloaded from www.ti.com/lit/zip/sloa208.
BoosterPack, LaunchPad are registered trademarks of Texas Instruments.
Arm, Cortex are registered trademarks of Arm Limited.
Bluetooth is a registered trademark of Bluetooth SIG.
Wi-Fi is a registered trademark of Wi-Fi Alliance.
All other trademarks are the property of their respective owners.
ALL_REQ
NFC-A polling command, equivalent to ISO 14443-3 short frame command WupA (0x52)
ALLB_REQ
NFC-B polling command, equivalent to ISO 14443-3 command WupB
APDU
Application Protocol Data Unit, used in command-response pairs to exchange I (information), R (receive ready) or S (supervisory) blocks.
ATTRIB
PICC selection command, Type B
ATQA
Answer To ReQuest A, ISO 14443-3 term, equivalent to NFC term SENS_RES
ATQB
Answer To ReQuest B, ISO 14443-3 term, equivalent to NFC term SENSB_RES
CC
Capability Container, contains management data and is stored inside a read-only EF file. This EF is located inside the NDEF tag application. Default (or basic) file ID for this file (for NFC) is 0xE103. See NFC Type 4 Tag Operation Specification and ISO/IEC 7816-4 for more information.
CE
Card Emulation, one of the three modes offered by NFC devices. In this optional mode of NFC operation, an NFC Forum device is considered to be a card emulation platform only when it is emulating a Type 3, Type 4A or Type 4B tag platform. Emulation of any other cards or tags is outside the scope of the NFC Forum Brand Promise.
DEP
Data Exchange Protocol, an abstracted operational layer that uses either ISO or NFC protocols to exchange data. Thus, two terms can be created with this acronym: ISO-DEP and NFC-DEP. In the context of this document, after activation and selection of the emulated card and before deactivation, ISO-DEP is used exclusively to exchange data between the reader/writer (PCD) and the tag platform (PICC).
EF
Elementary File, a set of data objects, records or units sharing the same file identifier and the same security attributes
File Identifier
2-byte data element used to address a file
fc
Carrier frequency, in the context of NFC/HF RFID, is 13.56 MHz ±7 kHz. This is the fundamental transmit frequency of the reader/writer (also called PCD).
Initiator
Generator of the RF field and source of the beginning of the NFCIP-1 communication
MIME
Multipurpose Internet Mail Extensions
Modulation Index, m
Signal amplitude ratio of [(peak – minimum) / (peak + minimum)] or [(1 – b) / (1 + b)], where b is the ratio between the modulated amplitude and the initial signal amplitude. The index, m, is defined per protocol type for both downlink and uplink and is generally expressed as a percentage (for example, Type A uses m = 100%, Type B uses m = 8 to 14%)
NDEF
NFC Data Exchange Format
NFC
Near Field Communication
PCB
Protocol Control Byte, used for conveying information required to control data transmission of blocks during the exchange of command-response APDU pairs. Bit coding of this byte and usage rules are found in ISO/IEC FDIS 14443-4.
PCD
Proximity Coupling Device (also commonly referred to as reader/writer)
PICC
Proximity Integrated Circuit Card (also commonly referred to as tag, tag platform, or transponder)
PUPI
Pseudo Unique PICC Identifier (randomly generated or static number returned by PICC as part of the response to REQB, WupB, ALLB_REQ or SENSB_REQ)
RTD
Record Type Definition
SAK
Select AcKnowledge (from ISO 14443-3), in NFC terms this is also called SEL_RES
SDD_RES
Equivalent to ISO 14443-3 response to SDD_REQ, and is complete NFCID1 CLn + BCC (if cascade level 1 (single size UID) or indicates NFCID1 is incomplete in the response and further cascade levels must be completed to obtain complete NFCID1+BCC.
SDD_REQ
Equivalent to ISO 14443-3 Type A anticollision sequence. Comprised of SEL_CMD, SEL_PAR and n data bits coded based on cascade level specified by SEL_CMD and calculated by value of SEL_PAR
SEL_RES
Equivalent to ISO 14443-3 SAK response
SENS_REQ
NFC-A polling command, equivalent to ISO 14443-3 short frame command REQ_A (0x26)
SENS_RES
NFC-A polling response, equivalent to ISO 14443-3 ATQA
SENSB_RES
NFC polling command response, equivalent to ISO 14443-3 ATQB
SENSB_REQ
Polling command, equivalent to ISO 14443-3 command REQ_B
Single Device Detection (SDD)
Algorithm used by the reader/writer to detect one out of several targets in its RF field (Type A anticollision, from ISO/IEC 14443-3)
T4T
Type 4Tag
Tag Platform
Responds to reader/writer (PCD) commands by using load modulation scheme (passive operation)
TLV
Type Length Value
UID
Unique IDentifier, a randomly generated or static number returned by Type A PICC as part of the response to REQA, WupA, ALL_REQ or SENS_REQ. It must be 4, 7, or 10 bytes long.