SLOA246B January 2018 – March 2019 TRF7964A , TRF7970A
All of the latest TI EVM and example firmware offerings are for the TRF7970A. Therefore, TI recommends using a LaunchPad™ development kit and a BoosterPack™ plug-in module for the TRF7970A for evaluation of all TRF79xxA devices.
For applications that need NFC functionality such as Peer-to-Peer mode, Card Emulation mode, or the ability to support reading tags that use NDEF for data formatting, the following combination of hardware and firmware is recommended:
For RFID applications that need to detect only NFC/RFID tags or read non-NDEF data from NFC/RFID tags, the following combination of hardware and firmware is recommended:
If it is not clear whether or not NDEF support is required, see Section 2.1 for further details.
The TRF79xxA devices covered in this FAQ guide are software compatible with the TRF7970A for the supported ISO/IEC and NFC standards.