SLOA248B January 2018 – March 2019 TRF7960A , TRF7962A , TRF7963A
All of the latest TI EVM and example firmware offerings are for the TRF7970A. Therefore, TI recommends using a LaunchPad™ development kit and a BoosterPack™ plug-in module for the TRF7970A for evaluation of all TRF79xxA devices.
The TRF79xxA devices described in this FAQ guide have only one firmware example that does not require any modifications. All other firmware bases need the modifications outlined in Section 4.1.
The aforementioned firmware example only supports basic RFID reader functionality, and the evaluation hardware that goes with it uses the TRF7970A device:
NOTE
The RFID Reader firmware example does not include full support for NDEF messages. For a TI example with full NDEF support, see Frequently asked questions for the TRF7970A and TRF7964A. If it is not clear whether or not NDEF support is required, see Section 2.1 for further details.
The TRF79xxA devices covered in this FAQ guide are not software compatible with the TRF7970A. See Section 4.1 for further details.
To evaluate the other TRF79xxA devices, it is possible to replace the TRF7970A on a TI EVM with the desired TRF79xxA device to help validate that the system, including firmware, is functional on TI hardware before producing any custom PCBs.