All trademarks are the property of their respective owners.
Smart speakers are always-on, waiting for commands and they spend most of their operation time in idle state. When in idle, these speakers are engineered to save system power, but the audio amplifiers used to drive them are usually less than 20% efficient at idle power levels. These amplifies are usually driven by single power level systems, so even while they are not driving a speaker, they are consuming significant power. TI has created an innovative architecture that can reduce not just idle power consumption by 90% but also improve efficiency by 15-20% at low levels of power without affecting the audio performance.
As shown in Figure 1-1, when Y bridge is being used efficiency is significantly improved at low power over the traditional use of PVDD supply.
![]() |
Black = Y-Bridge enabled Red = Y-Bridge disabled |
Traditionally the output stage of Class D amplifier is connected to single power supply, PVDD, which is usually connected to high voltage (2S or 3S battery or an output of boost converter). At low voltage levels of the output signals where headroom needed is much smaller than the available headroom, a lower voltage power supply can be used without degrading the audio performance. Since usually high and low voltages are already available in a system, the Y-Bridge power savings can be achieved without having to change the power architecture of the system. The TI Y-Bridge class D amplifier dynamically shifts between the high voltage (PVDD, for example, 10V-23V) and low voltage (VBAT, for example, 2.7 V - 5 V) rails based on the power needed to deliver the necessary output level. Figure 2-1 shows the functional block diagram of TAS2780.
The TAS2780 Class-D output uses a Y-Bridge configuration to improve efficiency during playback. The simplified schematic of Y -Bridge topology is shown in Figure 2-2. As can be seen, both PVDD and VBAT are supplied to the device and connected to Class D output stage. The power supply of output stage is divided into two separate paths, one path connects the output to PVDD and another path connects the output to VBAT. For low and idle level signals, the class D output is connected to the low voltage VBAT rail. This reduces the class-D output swing for small or near Idle signals and thus limits the power consumption of the output stage.
The device can be configured to enable or disable Y-Bridge feature. If Y-bridge mode is disabled, it will only use the selected supply for class-D output. Note clipping can occur if appropriate supply is not selected.
Y-Bridge feature automatically switches between PVDD and VBAT1S. When audio signal increases and crosses a programmed threshold, Class-D output switches over to PVDD supply. When in Y-Bridge mode, if the PVDD falls below a threshold level, the Y-bridge will stop switching between supplies and will remain on the PVDD supply. The threshold for switching between the two supplies is programmable by user.
When voltage levels at OUT_P and OUT_M are switching from 0-V to VBAT1S, the switching losses are much lower when compared to switching between 0-V and PVDD which results in increase in power efficiency.
While switching loses are reduced by using a lower voltage, the conduction losses increases as the VBAT1S path of the output stage usually is designed with higher RDS on to optimize the switching losses. At low output levels, the net power consumption is improved as switching losses are dominant of the two losses.
The TAS2780 can be configured to operate without an external VBAT1S supply, when an internal LDO is used to generate supply voltage at this pin.
TAS2780 can have different modes of operation:
The mode of operation can be set by setting the power modes registers (address=0x03 and address=0x04)shown in the Table 3-1 and Table 3-2.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7-6 | CDS_MODE[1:0] | RW | Oh | Class-D switching mode 00b = Y-bridge, high power on VBAT1S 01b = VBAT1S Only Supply of Class D 10b = PVDD Only Supply of Class D 11b=Y-Bridge, lower power on VBAT1S |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7 | VBAT1S_MODE | RW | Oh | VBAT1S supply 0b = Supplied externally 1b = Internally generated from PVDD |