SLOA332 july 2023 LMV821-N , LMV831 , OPA2991 , OPA345 , OPA376 , OPA376-Q1 , OPA377 , OPA377-Q1 , OPA4991 , OPA991 , TL074 , TLV376 , TLV9001 , TLV9002 , TS321
The peak slew rate of an output sine wave of frequency (f) and a peak-to-peak voltage (VPP) is shown in Equation 3. If the op amp slew rate is not high enough, then the sine wave becomes triangular with a reduced amplitude. For any output waveform, the slew rate is simply the first derivative of the waveform. From these methods the required slew rate can be determined.
For signals other than a step input, also consider gain bandwidth product (GBWP). The absolute minimum GBWP needed for an application is shown in Equation 4. For small signals on slew boost devices, it is recommended to use only GBWP for determining the sufficient op amp speed for a small input.
With the required SR and GBWP determined, consider how much of the input signal can be used as VID to generate that slew rate and gain. Choosing an op amp with much greater SR and GBWP reduces the VID required and potentially reduces distortion. Higher SR and GBWP come with higher quiescent current. For low power applications there is a compromise between supply current and AC performance.