SLOA341 October 2024 LOG300
A logarithmic amplifier approach is a way to achieve automatic gain control when dealing with input signals that are both high and low in amplitude. A log amp gains an input signal based on the log scale which helps get a stronger echo response from weak signals while also appropriately gaining the strong signals but preventing saturation, similar to the time-varying-gain approach. Whereas the time-varying-gain method is dependent on where an object is in time, the logarithmic amplifier is dependent on the actual echo of the input signal with no dependency on time.