SLOA341 October   2024 LOG300

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Description
    1. 2.1 Basics of Ultrasound Sensing
    2. 2.2 Advantages and Disadvantages of Ultrasonic Sensing
    3. 2.3 Ultrasonic Transducer
      1. 2.3.1 Transducer Construction
      2. 2.3.2 Transducer Frequencies
    4. 2.4 Transducer Topologies
    5. 2.5 Blind Zone Effect on Minimum Distance
    6. 2.6 Transducer Drive
    7. 2.7 Ultrasonic Echo and Signal Processing
      1. 2.7.1 Digital Gain or Fixed Gain
      2. 2.7.2 Time-Varying-Gain
      3. 2.7.3 Automatic Gain Control or Logarithmic Amplifier
      4. 2.7.4 Logarithmic Amplifier vs Logarithmic Detector
  6. 3LOG Detector Amplifier and the Advantages Over Conventional Opamps
  7. 4Application
    1. 4.1 Double Paper Feed and Paper Thickness Detector
      1. 4.1.1 Schematic Implementation
      2. 4.1.2 Material Thickness Detector
    2. 4.2 Bubble Detector
    3. 4.3 Material Detection
    4. 4.4 Distance or Proximity Detection
  8. 5Summary
  9. 6References

Transducer Drive

There are mainly two ways in which an ultrasonic transducer can be driven. The first one is the Transformer drive and second is direct drive and which type to choose mainly depends on the voltage requirement for exciting the transducer.

Transformer drive as the name suggest uses a step-up transformer to drive the transducer. The primary coil of the transformer is excited with low voltage signal and secondary side (which has a much higher voltage swing) drives the transducer. With transformer drive one can achieve the transducer excitation voltage beyond 100Vpp and so are generally preferred where the sound pressure level requirement is high like for application which requires measuring or detecting object at large distances.

Direct drive uses a H bridge (full or half) driver or an amplifier to directly drive the transducer. So in this the maximum excitation voltage is limited to the power supply of the system. These are mainly used for application where we don’t need large sound pressure level.

Type of mode to select also depends on the construction type of the transducer. Many open-top transducers do not require more than tens of volts to generate the maximum transmittable sound pressure level (SPL), so a transformer is not necessary, and a direct-driver mode is recommended. Closed-top transducers can also be excited in the direct-drive mode, but the transducers effective range is limited due to the typical requirement of hundreds of volts to generate the maximum transmittable SPL.

Table 2-3 Transformer Drive vs Direct Drive
Type Transformer Direct
Benefits
  • Able to maximize drive requirements for closed-top transducers (beyond 100Vpp)
  • Equivalent circuit enables de/tuning for short range
  • Fixed and tunable coil types available
  • Center-tap push-pull or single-ended available
  • Able to maximize drive requirement for open-top transducers
  • Able to drive closed-top transducer for short range applications
  • Half-bridge or full-bridge drivers available
  • Low-cost and small footprint
Drawbacks
  • Additional calibration and tuning required at mass production
  • High-cost and large footprint
  • Short range tuning limited to damping resistor