SLOA341 October   2024 LOG300

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Description
    1. 2.1 Basics of Ultrasound Sensing
    2. 2.2 Advantages and Disadvantages of Ultrasonic Sensing
    3. 2.3 Ultrasonic Transducer
      1. 2.3.1 Transducer Construction
      2. 2.3.2 Transducer Frequencies
    4. 2.4 Transducer Topologies
    5. 2.5 Blind Zone Effect on Minimum Distance
    6. 2.6 Transducer Drive
    7. 2.7 Ultrasonic Echo and Signal Processing
      1. 2.7.1 Digital Gain or Fixed Gain
      2. 2.7.2 Time-Varying-Gain
      3. 2.7.3 Automatic Gain Control or Logarithmic Amplifier
      4. 2.7.4 Logarithmic Amplifier vs Logarithmic Detector
  6. 3LOG Detector Amplifier and the Advantages Over Conventional Opamps
  7. 4Application
    1. 4.1 Double Paper Feed and Paper Thickness Detector
      1. 4.1.1 Schematic Implementation
      2. 4.1.2 Material Thickness Detector
    2. 4.2 Bubble Detector
    3. 4.3 Material Detection
    4. 4.4 Distance or Proximity Detection
  8. 5Summary
  9. 6References

Double Paper Feed and Paper Thickness Detector

Ultrasonic double feed detection technology is a sensor-based mechanism aimed to prevent multiple papers from being fed into a printer or scanner simultaneously. This not only increases the efficiency and accuracy of system’s operations but also contributes to preserving the integrity of the documents being printed or scanned.

This section provides an overview of the working principle of double paper feed detection and how the detection can be implemented using a log detector amplifier

Ultrasonic double paper feed detection works by using sound waves to detect the presence and thickness of paper in a feed system.

Transmitters and Receivers: The system consists of two ultrasonic transducers which are placed on either side of the paper feed path. One acts as a transmitter, emitting ultrasonic sound waves, while the other serves as a receiver.

  • Sound Wave Emission
    The transmitter sends out ultrasonic sound waves that travel through the air and hits the paper where a part of the sound wave gets absorbed, some gets reflected and while remaining permeate through.
  • Signal Reception and Detection
    The receiver picks up the transmitted sound waves. If there is only one sheet of paper, the sound waves can have a certain strength. When two sheets of paper are present, the paper absorb more sound energy, causing the transmitted signal to be weaker. When more than two sheets are there the signal is even weaker. The receiver detects this change in amplitude and based on that, the system determines whether a single sheet or multiple sheets have been fed into the machine.

This technology is crucial for preventing errors in processes that involve multilayer feeds, such as in printing or packaging industries, where the process makes sure of smooth operation and reduces material waste.

 Paper Detection Figure 4-1 Paper Detection