SLOK014A November   2018  – August 2024 TLV1704-SEP

 

  1.   1
  2.   TLV1704-SEP Single-Event Effects (SEE) Radiation Report
  3.   Trademarks
  4. 1Overview
  5. 2SEE Mechanisms
  6. 3Test Device and Test Board Information
  7. 4Irradiation Facility and Setup
  8. 5Results
    1. 5.1 Single Event Latchup (SEL) Results
    2. 5.2 Single Event Transient (SET) Results
  9. 6Summary
  10. 7SET Results Appendix
  11. 8Confidence Interval Calculations
  12.   References
  13.   B Revision History

Single Event Latchup (SEL) Results

During SEL characterization, the device was heated using forced hot air, maintaining the IC temperature at 125°C. The temperature was monitored by means of a thermal camera. The species used for the SEL testing was a Xenon (129 Xe) ion with an angle-of-incidence of 0° for an LETEFF = 50.5 MeV-cm2/mg. A flux of approximately 105 ions/cm2-s and a fluence of approximately 107 ions were used each run. The Vs supply voltage is supplied externally on board at recommended maximum voltage setting of 24V. Run duration to achieve this fluence was approximately less than 2 minutes. Three devices were tested at an output low condition where each device had a total of two runs.

Table 5-1 TLV1704-SEP SEL Conditions Using 129Xe at an Angle-of-Incidence of 0°
RUN #

DUT

DISTANCE
(mm)
TEMPERATURE
(°C)
IONANGLE

(°)

FLUX
(ions·cm2/mg)
FLUENCE
(# ions)
LETEFF
(MeV.cm2/mg)
24

3

70125Xe01.00E+051.00E+07

50.5

25

3

70125Xe01.00E+051.00E+0750.5

76

7

70125Xe0

0.997E+05

1.00E+0750.5

77

7

70125Xe01.01E+051.00E+0750.5

82

8

70125Xe01.01E+051.00E+0750.5

83

8

70125Xe01.01E+051.00E+0750.5

No SEL events were observed, indicating that the TLV1704-SEP is SEL-immune at LETEFF = 43 MeV-cm2/mg and T = 125°C. Using the MFTF method described in Section 8 and combining (or summing) the fluences of the two runs @ 125°C (2 × 107), the upper-bound cross-section (using a 95% confidence level) is calculated as:

σSEL ≤ 1.84 × 10–7 cm2 for LETEFF = 43 MeV-cm2/mg and T = 125°C.

 Run #24: DUT3 Supply Current vs. TimeFigure 5-1 Run #24: DUT3 Supply Current vs. Time
 Run #76: DUT7 Supply Current vs. TimeFigure 5-3 Run #76: DUT7 Supply Current vs. Time
 Run #25: DUT3 Supply Current vs. TimeFigure 5-2 Run #25: DUT3 Supply Current vs. Time
 Run #77: DUT7 Supply Current vs. TimeFigure 5-4 Run #77: DUT7 Supply Current vs. Time