SLOK017 June 2024 TLV1H103-SEP
PRODUCTION DATA
During SEL characterization, the device was heated using forced hot air, maintaining the IC temperature at 125°C. The temperature was monitored by means of a K-type thermocouple attached as close as possible to the IC. The species used for the SEL testing was a silver (47Ag) ion with an angle-of-incidence of 0° for an LETEFF = 48.47MeV-cm2/mg. The kinetic energy in the vacuum for this ion is 1.634GeV (15MeV/amu line). A flux of approximately 105ions/cm2-s and a fluence of approximately 107 ions were used. The supply voltage is supplied externally on board at recommended maximum voltage setting of 5.5V. Run duration to achieve this fluence was approximately less than 2 minutes. Two devices were tested where one device was biased in an output high condition and the other device was biased in an output low condition. Each device had three runs.
RUN # | DUT | Output Condition | DISTANCE (mm) | TEMPERATURE (°C) | ION | ANGLE | FLUX (ions·cm2/mg) | FLUENCE (# ions) | LETEFF (MeV.cm2/mg) |
---|---|---|---|---|---|---|---|---|---|
8 | 2 | Low | 40 | 125 | Ag | 0 | 1.17E+05 | 1.00 E+07 | 48.47 |
9 | 2 | Low | 40 | 125 | Ag | 0 | 1.18E+05 | 1.00 E+07 | 48.47 |
10 | 2 | Low | 40 | 125 | Ag | 0 | 1.2E+05 | 1.00 E+07 | 48.47 |
11 | 3 | High | 40 | 125 | Ag | 0 | 1.22E+05 | 1.00 E+07 | 48.47 |
12 | 3 | High | 40 | 125 | Ag | 0 | 1.18E+05 | 1.00 E+07 | 48.47 |
13 | 3 | High | 40 | 125 | Ag | 0 | 1.23E+05 | 1.00 E+07 | 48.47 |
No SEL events were observed, indicating that the TLV1H103-SEP is SEL-immune at LETEFF = 43MeV-cm2/mg and T = 125°C. Using the MFTF method described in Section 9 and combining (or summing) the fluences of the three runs @ 125°C (3 × 107), the upper-bound cross-section (using a 95% confidence level) is calculated as:
σSEL ≤ 1.23 × 10–7 cm2 for LETEFF = 43MeV-cm2/mg and T = 125°C.