SLOK017 June 2024 TLV1H103-SEP
PRODUCTION DATA
The purpose of this study was to characterize the effects of heavy-ion irradiation on the single-event latch-up (SEL) performance of the TLV1H103-SEP 5.5V, high speed comparator. Heavy-ions with an LETEFF of 48.47MeV-cm2/mg were used to irradiate the device with a fluence of 1 × 107 ions/cm2. The results demonstrate that the TLV1H103-SEP is SEL-immune up to LETEFF = 43MeV-cm2/mg at 125°C.
Characterization of single-event transients (SET) was also performed, up to a surface LETEFF = 50MeV-cm2 / mg at 125°C.