All parameters are measured according
to the conditions described in the Section 7 section.
Figure 8-1 shows the setup used to test the device's typical characteristics.
A. The 1 µF input capacitors
(CI) were shorted for input common-mode voltage
measurements.
B. A 33 μH inductor was placed in
series with the load resistor to emulate a small speaker for efficiency
measurements.
C. The 30 kHz low-pass filter is
required even if the analyzer has an internal low-pass filter. An R-C low pass
filter (100 Ω, 47 nF) is used on each output for the data sheet graphs.
Figure 8-1 Test
Setup for Typical Characteristics Graphs