SLOU559 April 2023
Go to the “Driver Control” tab.
Set the “Motor Driver” to “Awake” and the required stepper driver outputs to “Enabled”. (Enable either one output or both outputs at once to spin one or two motors respectively)
Select the desired “Control Mode” – This is a GUI app feature which allows selection between “Speed” mode and “Step” mode. In speed mode the motor can run at the set target speed using the defined acceleration and deceleration rate motion profile. In “Step” mode the motor can be stepped to the desired position by setting the required number of steps at the set target speed.
Features:
Step Mode: Can be used to set the microstepping mode
Full Scale Current: Can be used to set the full-scale current value
Starting Speed: The speed at which the motor starts spinning
Target Speed: The final target speed of the motor
Acceleration Rate: Set the acceleration rate at which the motor reaches the target speed
Stopping Speed: Can be used to set the stopping speed of the motor
Number of Steps: Sets the number of steps to cover
Steps to Stop: Sets the number of steps to stop
Reciprocate: Reciprocate the number of steps in opposite direction. Click 'Stop Steps' to stop the process
Fault Clear: used to clear driver faults.
Decay Mode: The Decay mode can be modified using the “Decay Mode” GUI push button in the STEPPER MOTOR CONTROL tab
Adjust the settings as needed and select “Start Input Based STEP” to start spinning the motor and use the “Input-based Direction” to change motor direction.