SLOU563A april 2023 – september 2023 TAS6424R-Q1
When the TAS6424E EVM PPC3 is launched, the Home Window is shown. If the EVM is powered on and the USB is connected to the PC, then the Home Window displays the Connect box in the bottom right hand corner. If the EVM is not powered on or the USB is not connected, then only the TAS6424E EVM – Offline is displayed.
Figure 2-4 shows the downloading progress of TAS6424E application.
There are three windows available with the TAS6424E EVM PPC3: Home Window, Register Map Window and Device Monitor, and Control Window.